According to the standard the Q-factor of the receiver coil should be at least 77.
According to the TIDA-00329 a the Würth 760308101303 coil would meet these requirements. But according to the datasheet of Würth the coil only has a Q-Factor of 25 (which I have no idea how the calculated it, because based on their other datasheet value the Q-factor would be somewhat above 77 in an ideal case, and below 77 if you're unlucky).
But when I look on e.g.
www.mouser.ch/.../
Many of this coils are far away from a Q-factor of 77.
So I wonder if we still can use a bq51050B with one of this coils.