This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

INT-Does TPS53317 support VREF?

Other Parts Discussed in Thread: TPS53317, TPS51200

Does TPS53317 support VREF?

Customer use TPS51200 to support VTT rail and TPS51200 can also output VREFas pin 6.

They use VREFOUT as pin 6 to connect to their DDR.

For new project, the need the current rating of DDR termination higher to 4A. So, I propose TPS53317 to them.

But, TPS53317 didn't output VREFOUT pin.

For this application, could we use TPS53317 support this case which need VREFOUT?

if yes, how to connect it?

if no, do we have any suitable solution can propose?

thank you in advance!!

BR,

Jason