Hi,
Is it possible to use the BQ24616 without connect it to the system? the charger will be use only for charge the batterie. That mean the BATFET will not be monted and the system will not be connected to the charger.
Thanks
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
Is it possible to use the BQ24616 without connect it to the system? the charger will be use only for charge the batterie. That mean the BATFET will not be monted and the system will not be connected to the charger.
Thanks
Hi Steven,
Thank you for this information. If i don't connect the system, i can replace the resistor betwen ACN et ACP by an 0Ohm?
Thaks
Clément