Hi
I need help to select the correct chokes when I use the UC2843 and UC2800. the output is 27, the input can be 11 to 36 volts, the current is 2 ampers
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
I need help to select the correct chokes when I use the UC2843 and UC2800. the output is 27, the input can be 11 to 36 volts, the current is 2 ampers