Hi,
I'm using the bq24610 in an application where I need to disable termination, precharge and DPM (adapter current regulation). Disabling termination is explained, tie the timer pin low.
With termination disabled, can I simply program Iset2 for approximately the same charge current as Iset1 effectively disabling precharge?
To disable DPM, can I simply connect ACP to ACN? What do I do with ACSET, ground it or float it?
BTW, I do need the power path control but I don't need adapter reverse protection (input will be hard wired). Do I still need both input FETS?
Thanks,
Marty