I have designed a custom board running Linux with the bq27421G1B gas gauge. I am able to read parameters correctly from the device, however I have not done any calibration for it. I do not have the evaluation board, only my custom board. Can I use the bq studio app somehow with my custom board? Is there an adapter that I can rig into the I2C bus, and run bq studio from windows?