We have an LM3509 driving two sets of two white LEDs.
With L = 4.7 uH and C = 2.2 uF, we had the output voltage at 21.3 V and the LM3509 got hot (over 50 C)
Switching to L = 4.7 uH and C = 22 uF, the output voltage went to 7 V so we should be dissipating less heat on the LM3509. But it still heats up to 50 C, and is dissipating 500 mW. How to reduce this? The diode is Diodes Inc SD103AWS-7-F