This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Battery Charge ISSUE

Other Parts Discussed in Thread: EV2400, BQ27531-G1

Hi, I'm trying to manage one bbattery charge of 10000mAh, I'm using bq27531 and a EV2400 to communicate to the computer, the software that I'm using is the one that you download from the internet page (. well, i left the battery charging for a while and in the battery porcentage never change, but when I discconect the battery and connect it again the battery minitor goes to 0% and then change to the real battery charge, for example, the battery start on 66%, left it charging to 600mA for 3 hours and it doesn't change then I discconect the battery from the bq27531, left the software to arrive to 0% and then reconnect the battery, and now the battery in on 69%. other thing, the software is reading all the parameters each second(option Keep scanning).

Integrar imagen