Dear Support Team
Could you provide any actual value data of VHI,VLI pin pulse voltage tolerance?
It is helpful if you can provide below data.
◆Conditon
-5V/500ns pulse applied VHI,VLI pin
Regards
Tomohiro Nagasawa
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello Tomohiro,
For the VHI and VLI pins, I am not seeing the pulse rating for the voltage on the pins. The VHS, VHO and VLO have pulse ratings as shown in the Abs Max Rating table which are implied as maximum time and voltage.
Are you referring to the VHS, VHO or VLO pins?
For the UCC27201 LO and HI pins there is an EDS protection cell which limits the pin voltage to ~ a diode drop below ground. The negative current needs to be limited with a series resistance. For -5V a series resistance of 500 Ohms will limit the negative current, if that is OK in the application.
The UCC28711 driver input is specifically designed to tolerate -10V on the LI and HI pin inputs. The best recommendation would be to use this part for negative voltage tolerance on the LI and HI pins.