This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DCP010515BP-U / connecting in 6 parallel

Hi,

My customer is asking if DCP010515BP-U can be used in 6 parallel operation. Please let me know also the precaution for use with such a number of paralleling.

Best Regards,

Sonoki / Japan Disty

  • Sotoshi:

    The DCP010515BP current sharing has only be confirmed to 2 DCP010515BP. They only current share based upon the unregulated operation where Vout varies as a function of output voltage versus output load.

    Tom 

  • Hi Tom,

    Long time no see !!
    I understood that it has been confirmed to two parallel operation and so you can recommend up to two paralleling. I asked it because it's stated "it is possible to parallel the outputs of multiple DCP01Bs" in datasheet.

    Best Regards,
    Sonoki