This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PMIC for Following requirement

Other Parts Discussed in Thread: TPS65250

Hi,

Is there are any PMIC for following requirement.

Vin Nominal =12V, Min=6V, max=18V

outputs:

1. 3.3V @300mA

2. 5V @ 130mA

3. 12V/9V/6V @2mA

4.  1.8V @ 20mA

5.  3.5V@ 400mA

  • Hi Ranganadh,

    Is rail 3 (12V / 9V / 6V) a buck boost or does the output go down as the input goes down? How does it know to change between the three? I2C communication or the way external feedback is setup?

    Something like the TPS65250 might be a good option for the 5V/3.3V/3.5V rails with two discrete LDOs for the other two