Dear Designer and TI support,
I'm evaluating the TPS92640 for a LED driver application where multiple regulators and different LED string are used. At the moment I'm using the TI demo board, with the following load / input specs-
Vin = 48V
nLED = 8
VLEd = 3V for a total Vout of 24V
ILED = 0 to 700mA
I used the demo board TPS92614EVM with 2 different configurations:
1) The original configuration where I only added the R11=1.2M of the demo board (Is the RFOO of the data-sheet) for a true zero current LED operation and I've cut R5 of the demo board, connecting an external signal generator to IADJ pin . Setting the VIADJ to 541mV the real measured current through the LED (I used a multimeter) is 242mA instead of 541/2= 270m . So apparently there is a static error in the regulator loop
I've noticed that connecting just 4 LEDs no static error occurs.
2) I've redesigned the board to support 8 LED Vout = 8*3=24V Vout just changing 2 resistor values R7 = 200K (Rvout1) and R1 = 20 K (Ron). R5 is cu and a signal generator is connected to the IADJ pin. R11 is always set to 1.2M and the rest of the components remain the same. Unfortunately static error occurs again
Even without any R11 resistor in both 1,2 configurations the static error occurs.
Any Idea about the reason of the above problem ?
Thanks and regards
Paolo