This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ24232 Problem with charging

Other Parts Discussed in Thread: BQ24232

Dear TI-community,


We implemented the BQ24232 in a design but have a problem with charge output voltage. When 5V,500mA are applied to the Input Pin,  we measure a voltage of 0.7 V (instead of 4.2 V) at the BAT Pins. Output voltage is correct.

We want to charge with 200mA and used the circuit described in the datasheet. Please find attached our schematic.

Do you have any hint where these 0.7V come from? Or is there a mistake in our schematic?

We are looking forward to your reply

Kind regards,

Karina