Dear TI community,
I am designing an LED lighting system for my aquarium. I am planning to use the following RGB + W LEDs (RS part numbers given below)
897-8825 x 10
897-8813 x 10
897-8819 x 10
791-9838 x 10
Now from the datasheet of this LEd driver, it mentions that in one chain, we can connect 1 - 3 LEDs.
so here is my question.
If I have a CV supply of 24VDC, 60W, can I run more than 3 LEDs in one chain?
I am controlling the LED driver using a PIC and PWM.
Many thanks
Mat