My application is an autonomous electric vehicle with an embedded host processor. I need to read/write SBD commands directly to the chip, no bqWizard, no API. The SBS Command values listed in tables A.1 and A.2 of the tech reference (SLUU330A) do not cover all parameters that are available from the chip. For example, there is no documented SBD command to read cell temperatures. I am monitoring the SMBus communications between bqWizard and the bq78PL114, and I can see that the wizard is using block write and block read commands to communicate with the chip. Can anyone provide me with the formats for the SBD block commands for the chip? Also, can anyone point me to some documentation on SBData command mapping for the bq78PL114, or explain how to interpret the the information provided in the SBData Command Mapping utility within the bqWizard?
Thanks, David