Other Parts Discussed in Thread: LM2936
Dear TI Engineers, there are two grounds, pin 2 and pin 3 as well as pin 6 and pin 7 per side of LM2936M SOIC (D) Package. Why do I need two grounds? I am trying to adhere to 2mm spacing, and I would like to only use one ground per side in my 4-20mA 24V Intrinsically Safe (IS) application? Do you see a problem? What are the ampacities on the leads, etc...???? Why were two grounds provided in the first place.
Additionally, historically, we have not a Cout (output capacitor)--we assume this is no problem, correct? This just affects our stability, and we are fine with stability, correct? Thanks for your help! Best Regards, Rohit