I have a circuit using the TLV62130 to charge a battery. The input voltage is 5.0V and output is 4.0V. The input current is 1.5A, and the output current is 1.5A. I expect the efficiency to be a little higher. As a result the chip rises 45C over ambient even though it's connected to a ground plane. This is consisten with the thermal resistance in the datasheet: (5V - 4V) * 1.5A * 29.1 = 44C rise.
My question is why I'm getting only 80% efficiency and how I can dig into the circuit and find what I'm doing wrong.
CJ Gervasi (No relation to the CJ in Austin) :)