This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LP3891-1.2 do not produce 1.2V.

Other Parts Discussed in Thread: TMS320F28377D

I have LP3891EMR-1.2/NOPB.

I intended to supply 1.2V to TMS320F28377D by using LP3891EMR-1.2.

But, it does not work properly. It produces 2.6V fixed voltage, instead of 1.2V.

Here is my pin connection. The package type is SO PowerPAD-8. 

I provide 5V to pin 3.

Pin 4,5 are connected to GND properly.

Pin 6,7 are tied together and I supply 3.3V to them because I don't want to use shut down function.

In this configuration, I expected 1.2V to pin 1,2. However, it was 2.6V.

What's wrong? Do I understand the regulator mistakenly?

Thanks for reading.