This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

bq27421g1 a -variation is soc if i restarted the system

When my system is connected to battery it shows suppose 5%.

If i connect the adapter there is a voltage variation but there is no change in the battery percentage.

But if i poweroff the system and restarted it shows some 15%.

why is it so:/

how can i avoid it?