This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS6206x loop stability

Other Parts Discussed in Thread: TPS62067, TPS62097, TINA-TI

Hello,

I need to smoothen the ramp-up time of Vout to less than 1V/ms for the TPS62067. I am using the Switcher Pro to make a quick design but the recommended Cout is 22uF, which is good enough for the LC network and loop stability, but my external supplied circuit has additional decoupling capacitors and I have to add and additional 470uF capacitor to smoothen even more the ramp-up time when the converter is powered up.

Is the circuit recommended by TI (WEBENCH, Switcher Pro) good enough, taking into account that the external circuitry has additional decoupling capacitors and a 470uF capacitor to smoothen the ramp of the transient power-up? By adding additional capacitors, the stability of the converter is put in jeopardy?

Thanks.