Hi,
I am using TPS386596 for generating Power On Reset for the processor. The power lines needs to be monitored are 3.3V,1.8V,1.35 & 0.9V .As per the datasheet 3.3V can directly connect to sense 1. For others I need to use resistor dividers .The formula shown in datasheet is VMON = (1 + RSnH/RSnL) × 0.4 (V)
But the resistor values shown in "Detailed Design Procedure" page 13 ,table 3 are not matching with the equation provided.
For eg for sensing 1.5V rail ; RSH = 25.5K & RSL = 10 kΩ ( As per equation it will be RSH = 27.5K & RSL = 10 kΩ )
Also in table 3 mentioned about RS4M = 1K but nowhere explained What is RS4M
Please clarify these doubts...
Regards,
Leo