Hi,
I have a problem with TPS 23861, have five controllers connected in daisy chain, and I want to work in automatic mode, four of them working correctly but one does not work well.
By I2C link, I have assigned different directions and all respond correctly to the assigned address.
The problem is that when I write in the register "Reset 1A" (0xD0) Four are configured in auto mode "Operating Mode 12" (0xFF) but the fifth this register has to (0x00).
I have found that in the "Device ID 43" the content of the four operating in automatic mode is (0xE3) but that is not configured in automatic mode content is (0xE2)
Can this be the problem?
Thank you