This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS62730

Guru 13485 points
Other Parts Discussed in Thread: TPS62740

what is the max. current that can pass thorough the FET bypass to the load?

  • We can use the part’s 100 mA rated current as a limit. But note that the bypass switch has a high Rdson which will cause a voltage drop—this can be significant at higher currents.

    As well, there is the TPS62740/3/6/8 instead. These don’t require an MCU to control the low-Iq mode and provide higher efficiency in most applications.

    We can continue on email, if you prefer that way.