Hi,
I am using the LM5119 evaluation board. When I changed the feedback voltage divider on the 10V output I got a much lower voltage out than expected, so I reverted the change and put the original resistors back. After doing that, the output was about 5V but not stable and if any load is applied the controller shuts off. I have looked into it to some extent, but was hoping someone more knowledgeable could help me pin down the problem.
Thanks,
Mitch