Hi Team,
Our customer would like to use only negative output voltage(OUTN).
Because, they would like to regulate the negative output voltage in little BOM.
Do we have to connect C4 even if we don’t use OUTP?
They removed C4(output capacitor of OUTP).
Then, this device can't output the target negative output voltage(OUTN= -5.0V).
(So, this output voltage was “-4.7V”.)
[Conditions]
VIN=3.0V to 4.2V
VOUT=-5.0V
Iout=1mA
Regards,
Kanemaru