Dear TI's FAE,
Please help to reply the below two questions. Thanks !
1. the definition for BOOT1 pin ? (not described in TI's docs)
2. When the WR_S bit is 0, reload the default VSEL[5:0] value when a warm reset occurs.
The default value VSEL[5:0] is from EPROM and will be the voltage from 0--> default voltage(if 1.8V) or current voltage setting(2.0V) ---> default voltage(1.8V) ?