Other Parts Discussed in Thread: BQ24253, BQ24250, BQ24297, BQ24190
Hi,
We are planning to use USB charging and would like a product that could detect the charging source to determine the correct charging current which can be anywhere from 100 mA to 1.5 A. Is there such a device?
I've looked at the BQ24253 and the BQ24250 but it looks like I need some external circuitry to detect and set the EN pins correctly.
Cheers
Calum