HI,
We are designing a wireless charging solution. The charge current requirement is 50mA in my application. Hence the combination of the bq51003 wireless receiver and the bq25100 low power linear charger will be used as recommended in e2e community.
Would need your recommendation on the following options:
1. Recommended Tx solution for use with this receiver.
2. Can the bq500511 & bq50002 solution be used?
3. Else should I go with bq500210 part which is recommended in bq51003.