Hello,
We are looking at using the TLC59116 in our design, but can't figure out what VOL stands for. Our assumption is that it is the dropout of the device, but what is the value of VOL? It is referenced in the datasheet as follows.
Figure 2 shows the output voltage versus the output current with several different resistor values on REXT. This
shows the minimum voltage required at the device to have full VF across the LED. The VLED voltage must be
higher than the VF plus the VOL of the driver. If the VLED is too high, more power will be dissipated in the driver.
If this is the case, a resistor can be inserted in series with the LED to dissipate the excess power and reduce the
thermal conditions on the driver.
Any clarification would be helpful.
Thank you