Hi,
I am working on using the TPS5430 to shift from 12-15V to 3.3V. My output current is relatively low, most likely not exceeding .5 A. The smaller the current, the bigger the inductor needed. Using the datasheet and corresponding equations, an inductance of 63uH and a capacitance of 80uF for the output capacitor would work according to calculations. I double checked this with Switcher Pro, which yielded 120uH and 180uF respectively. The inductance is a minimum, so I don't want to use too small of an inductor, but the datasheet also states inductance values for use with this chip typically range from 10 to 100uH. I double checked the example used in the datasheet with Switcher Pro, and it yielded larger values as well (Switcher Pro said 27uH and 470uF vs. the packet's 14uH and 220uF). I don't want to use too large of an inductance value, but I definitely don't want to end up too low. Anyone have any recommendations? Is it possible to go too high with the inductance or should I go like 150uH to be safe?
Also, after using Switcher Pro, I checked what the crossover frequency would be with the packet. The math says 4.18kHz, but Switcher Pro says 5.1kHz on the Bode plot. I guess this is just yet another discrepancy between Switcher Pro and the packet. My bigger concern was that my zero ESR frequency for my circuit (15 to 3.3V @ .5 A) was 176.8kHz, which seems very high. This was taken from the Bode plot on Switcher as well. The packet said zero ESR should not be too far above compensation poles @ 24k and 54k.
Perhaps Switcher Pro isn't very accurate. But I don't know, which is why I'm here asking. Specs for my situation are 12-15V input, 3.3 V out, approx. .5A max load on the output. Any help on what I should use or suggestions would be much appreciated. Thanks.
Chris