I have a customer with the following question:
In working on the MPPT hardware, I am looking at doing something like in the App Note SLVA345A, Figure 2. However,...
(1) The tps61200 is only unidirectional, correct? I.e. there is no condition during which my output can discharge back into the tps61200's output pin and toward the Vin source?
(2) Regarding the MPPT function, is the R4 divider at OPA379 + terminal input supposed to be set for the PV cells MPP, or for a low voltage cutout threshold?
(3) Finally, this report states the MPPT circuit was tested with a variety of solar cells. Can a table of a couple examples be included? For example, the PV cell in Figure 1: 0.6Vmax, 0.5V MPP, say 0.4Vmin (operating), what was the R4 ratio for this cell? Although, this cell was obviously a fair size, and the tps61200 isn't capable of delivering all the current it can supply to a load, right? This actually brings up another questions:
(4) the 'short circuit' current protection would also act as a over-current protection (in the case of the 5A PV cell capability), correct? What will it limit the input / output currents to, ~1.3A device current rating??
Can you help??