Hi
I have a question about LM317.
Is that possible to disable(ADJUST pin=Low) by the ADJUST pin?
Regards,
Koji Hamamoto
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Koji,
For the LM317, the lowest Output voltage that you can have is 1.25V. So even if you connect the adjust pin to ground it will still output 1.25V.
I suspect that you are trying to make a switch from the LDO? There are a few other LDOs that have an enable pin such as LP2985 and LP2951.
If you provide me with more detail about your parameters I can try to help more.
Thank you,
Cameron Phillips