This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Isolated DC/DC converter that meets 2 MOPP specifications

A customer is requiring isolated DC/DC converters that meet the IEC60601-1 3rd edition standard noted as Means of Patient Protection (MOPP). Below is the isolation, creepage and insulation requirements for MOPP.

2 x MOPP

  • Isolation: 4000 Vac
  • Creepage / Clearance: 8mm / 5mm
  • Insulation: Double

If anybody can suggest isolated DC/DC converters that meet these requirements, it would be much appreciated.