Hi there!
According to the data sheet, one has to Options to supply the VIO rail:
- use SMPS9
- use an external 3.3V supply controlled by REGEN1
For my design, I chose the second approach. Therefore, SMPS9 output ist not used in the design.
Which is the proper way to treat SMPS9?
- as in the EVM: supply SMPS9_IN, leave SMPS9_SW and _FBK open and connect SMPS9_GND to GND
- as in the TPS659037 Design Checklist: supply SMPS9_IN, leave SMPS9_SW open and connect SMPS9_FBK and _GND to GND
- probably something completely different like not supplying SMPS9_IN
Thanks in advance
Wolfram Stumpf