Hello,
I am trying to use (3x) TPS65131 split-rail DC/DC Regulators in my senior design project to supply 6 different voltages off of my power board (+9V/-9V , +5V/-5V, and +3.3V/-3.3V). I am using the typical application set-up as shown in the datasheet with the necessary adjustments (R1, R2, R3, R4, C9, and C10) needed to achieve the desired voltage outputs as explained in the datasheet. However, I am not including the transistor in my design, but I do not think that is my problem. After calculating the R and C values for the corresponding voltages and using components that are fairly close (within 5%), I am not getting what I am trying to achieve. For the +5V/-5V system, I am getting an output of 15V/-11V respectively... For the 3.3V/-3.3V system, I get +5V/-3.2... And for the +9V/-9V system, I get an output of +8V/-11V. Some of the outputs are close to what I need, however when I try to compensate the difference (tuning the resistor values) to get closer to my desired outputs I have to change the resistors drastically (change R1 from 1Mohm to 10Mohm) in order to reach +9V for example. The main issue here is that when I change R1 to 10Mohm, the Positive Feedback Regulation exceeds 2V which is not in range as stated in the manual. Also, When I connect a load to either the +9V or -9V output, the voltages on the outputs drop to +5V and -0.2V, respectfully. I cannot seem to figure out why I am getting these inconsistent results. What could I possibly be doing wrong? HELP!
I have attached my Altium schematic, including component values, with this post.
Thanks!
Courtney Smith