I have a question.
Question is Switchig MOSFET's allowable power dissipation.
My cusotmers are considering a set of LM5116 + CSD19534Q5A.
So, I want you to tell me the loss data calculation method of CSD19534Q5A.
I used a webench designer.
But,It did not work.
They want to use the MOSFET in parallel.(Highside = 2chip, Lowside = 2chip)
Because,Output current is large.
<This is customer's spec.>
Input Voltage:50V
Output Voltage:12V
Output Current:12.5A (150W peak)
Highside:CSD19534Q5A × 2chip
Lowside:CSD19534Q5A × 2chip
Do you have a method of calculation or calculation tool?