This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Shut down temperature in TPS40057

Other Parts Discussed in Thread: TPS40057

Hi

Please tell us about the junction temperature of the TPS40057.
TPS40057 Datasheet (RevI) Page4
Max junction temperature 150℃
”Device may shut down at junction temperatures below 150℃”

What degrees is the temperature to shut down?
Not guaranteed value, Customer wants actual values.

I want also the approximate value.

This is because competition MPS MP2908A is junction temperature 150 ℃.
The higher the priority of the junction temperature in the safety-oriented.

Best regards,

Mitsuo Hirata