This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS65400 INDUCTOR value for SW2 to generate 5v at 2A



For SW2 & SW4:

I have used 6.8uH for SW2 to generate 5V o/p @2A. used (24.9K + 100 ohm) as R1 & 10K as R2

Inductor used: RLF7030T-6R8M2R8 from TDK, Irms=2.8A, L=6.8uH ±20%, is this inductor & resistor values are right? Can any one confirm this? Please send me the answer ASAP. Because I need to release the design files for PCB fabrication. Thank you very much