Hi,
I am using a TPS65381 for TMS570LS3137, we used VDD1sense as tms570LS3137 VCC core supplier which the input voltage is 1.2V.
from TPS65381 datasheet, i can find the maximum output VDD1sense current is 600mA, but from TMS570LS3137 data sheet, TI No. SPNS162, TMS570LS3137 PBIST mode consumes 700mA current.
so my question is:
1, the output of VDD1sense is from 0.8V---3.3V, whether the output is always 600mA, or the output current is a variable based on output voltage;
2,could we used tps65381 as tms570ls3137 power supplier?
thanks!