Hi Team,
My customer is considering using TPS7A88.
He would like to use it under the following conditions.
Vin:1.8V
Vout1:1.1V
Iout1 max:1.1A
Vout2:1.1V
Iout2 max:0.34A
operating temperature range:-40~85℃
Please let me ask you two questions.
Q1)The max 1.1A of Iout1 current is his requirement.
Is TPS7A88 possible to use under that conditions?
Q2)He would like a Load Regulation data(Vin=1.8V,Vout=1.1V,
Iout max=1.1A,Ta=85℃,105℃).
If you have a useful reference data regarding the above conditions,
could you please share it with me?
Best regards.
Tsuyoshi Tokumoto