This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS61071 In Parallel

Other Parts Discussed in Thread: TPS61071, TPS61291

Hello, I need to be able to generate 3.3V at 250mA from a 2V source.  I was wondering if I could put two TPS61071 in parallel to achieve that.  Both chips will have the same VBAT and both ENables will be tied together so that both chips start at the same time.  Is this as simple as connecting the two outputs together?  Could you suggest a better solution to my problem?

Regards