Hi all,
I use a TPS65100 for a LCD panel.
All the voltages have the values, they supposed to have.
Only the positive voltage (Vout3) is higher than expected. Also the Fb voltage (1.21V - datasheet) is higher -> 1.38 to 1.4 (spread of 5 PCBs).
There is no load on the outputs! res divider on V3 is 470k/27k.
Does the ref voltage Fb3 change if you load any of the outputs?