I need to design a PFC circuit for 1200W high intensity discharge light ballast, with 400VDC output.
I have seen UCC28061 used, but the datasheet suggests that UCC28061 not used for loads over 750W. Exactly why is UCC28061 not ideal for loads over 750W?
Would UCC28070 be a better choice?
Ideally, the PFC would operate between 120-277VAC. Other than making sure passive components can handle the extra volts, is there anything I can do to get these PFC IC's to handle 277VAC input?