This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LP5521 CLK_32K input specification



There are no min/max frequency specifications for driving the CLK_32K pin. What are the limitations? Experimentally, I found it still functions above 3 MHz, so I assume operating around 100 kHz should be OK.