Dear Sir,
I have designed a quadruple GNSS (Global Navigation Satellite System) Radio-Frequency Front-End, i.e. four RF super-heterodyne independent RF channels in a single Front-End. Then I use a four channel ADC to digitize the four IF signals.
The main supply voltage is 5v, and the total consumption is high (including RF circuitry, ADC, and FPGA board).
So, first I use a high efficiency switched power supply (LMZ21701) to generate 3.7v from the 5v. Then I use LDOs (LP3982) to generate 3.3v from the 3.7v. In fact I use 3 LDO (at 3.3v s per each channel, one for the LNA (Low Noise Amplifier), a second one for the LO (Local Oscillator), and a third one for the VGA (Variable Gain Amplifier), which yields a total of 3x4 = 12 LDOs!!!. I also use ferrite beads. The noise in the power supply is low. However I believe my design might be too redundant. My questions are:
Are LDOs a good solution to filter out the noise and glitches coming from the switched power supply? I guess that not really, as far as I know they behave as a High Pass Filter. They will filter out the low frequency oscillations, but the noise due to the switching inside the switched power supply is above their cut-off frequency. In fact ferrite beads should be more efficient for this purpose. Do you agree?
It is wise to supply RF circuitry (LNA, PLLs, VGA) from a switched power supply (LMZ21701) carefully filtered by ferrite beads and capacitors?
Using one independent LDO for each RF blocks will be helpful to reduce crosstalk among RF channels? Again I guess it will not, for the same reason aforementioned. Do you agree?
What about supplying the ADC with a second (LMZ21701) to generate 1.8v from the incoming 5v (again, carefully filtered by ferrite beads and capacitors) ?
BR
Orlando Peña