This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

bq25505 VBAT_OV threshold accuracy

Other Parts Discussed in Thread: BQ25505

On the bq25505 datasheet, VBAT_ACCURACY is +/- 2% with 0.1% resistors.
When 1% resistors are used, how is the accuracy?

According to my calculation, I think it becomes about +/-3%. Is this right?

Best Regards,
Kohei Sasaki

  • Sasaki-san,

    Please use this app note to look at impact of resistor tolerances. www.ti.com.cn/.../slva423.pdf

    You can also calculate the VBAT range with the lowest and the highest of the two resistors.

    Regards,
    Gautham
  • Gautham-san,

    Thank you for your answer.
    According to my calculation, the accuracy becomes -0.5% and +0.7% from VBIAS and resistor tolerance. However Electrical Characteristics is +/-2%. Thus I think we should add -1.5% ans +1.3% value to calculation result.
    So the threshold accuracy becomes +/-3.3% with 0.1% tolerance resistor.
    Is my understand correct?

    Best Regards,
    Kohei Sasaki