I have a LED driver that takes 50V DC and draws max 7.2A . I want to detect if the power supply fails but since this driver is PWM when I dim the LEDs the input current drops to 10mA .
do you have a chip that can either detect the break in current or the current dropping below a certain limit.
or the other possibility is that if a chip can give me analog value related to the current I can read it in my micro controller and generate alerts.
thanks