This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS65150 test condition VCOM current

Other Parts Discussed in Thread: TPS65150

HI,

We are using the TPS65150 and we are wondering what is the maximum output current that the component can provide on the VCOM signal?

We used a configuration to get on Vs 9.3V, VGL -10V, VGH 15V and VCOM 4V.

In a test, we want to know if the component can provide 100mA dc on the VCOM pin. To check it, we add a 40Ohm charge resistance on the VCOM pin. The VCOM signal drop to 1.21V. The Vs, VGL and VGH voltages are still correct. In the datasheet, it seems that the TPS65150 can provide at least 150mA.


Do you have any idea why we get this result?

Thank you in advance,
Best regards,

Sébastien