I have a legacy design that is driving the sense pin (CS) of the UCC2807-2 slightly negative. I understand that the "voltage rating" is -0.3V to Vdd+0.3V. I want to know if there is an associated current limit value? Also, I am concerned that that the CS feedback going negative impacts the operation of the current mode control. I do plan to correct the design, but I want to understand the current configuration.