I just got the EVal board and based on the document SLUU904A, there is a specific tool for the bq34z100 device that I can download under
There is also the more general Battery Management Studio. So which one should be used?
Thanks.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I just got the EVal board and based on the document SLUU904A, there is a specific tool for the bq34z100 device that I can download under
There is also the more general Battery Management Studio. So which one should be used?
Thanks.
Hi Thomas,
Actually I already have bqStudio downloaded. My question is there are two software programs for this chip.
One is specific to the chip which can be downloaded here:
I was using the EVAL board so I assume the firmware has been programmed. But even with the warning message, I was able to use the bqStudio and read/write register. When I read back "DEVICE_TYPE", I got back 0x0100. FW_VERSION is 0x0006. HW_VERSION is 0x0080.
I mean I can either use both software tools and read/write registers OK.